Cancel
Showing results for 
Search instead for 
Did you mean: 

PC Hardware for Robcad

Experimenter
Experimenter

Hi,

 

Currently we have HP Z200 with configuration like this:

 

Processor: Intel Xeon CPU X3440 @2.53 GHz 2.67 GHz
Installed Memory (RAM): 8GB 1333 MHz
GPU: NVIDIA Quadro 600 (Dedicated Memory: 1024 MB, Shared System Memory: 3807 MB)
Storage: 7200 RPM, RAID 1

 

We have serious performance issues with this configuration. What we need is to simulate cells with 10-15 robots. When we check the certified hardwares from HP, we see there are several variations. What must be our specifications to simulate these kind of cells? Do we need SSD? What must be the cpu and gpu details? Any help will be appreciated.

 

Thanks,

2 REPLIES

Re: PC Hardware for Robcad

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

hi,

 


for a big cell is the "Tianhe-2" (Supercomputer) a good solution.  Smiley Very Happy Smiley Very Happy Smiley Very Happy Smiley Very Happy Smiley Very Happy

 

joking....

 

a DELL Precision M6800 with big CPU and Geforce K4100 nvidia card is a good solution.

SSD harddrive is good for loading speed.

 

Kind regards,

Benjamin Voelzke

Re: PC Hardware for Robcad

Experimenter
Experimenter

Hi,

 

Thank you for your help. If it is possible could you also name a non-mobile configuration?

 

Best Regards,