Cancel
Showing results for 
Search instead for 
Did you mean: 

PS Application Starting then Immediately shuts down

Builder
Builder

Hi All

 

I have an issue on one of our Standalone Machines, wehre i start tecnomatix PS, the application boots then shuts down immediately. 

 

Any one have an idea what it could be?

 

We are running PS 13.1.0

NX10.3 Win10 64bit, Tecnomatix PS V13.1.
2 REPLIES

Re: PS Application Starting then Immediately shuts down

Legend
Legend

Hello!

 

The case explained is that the PS main booting screen appears, but the application window  does not right?

 

One thing to try: In your "C:\Users\YourUserName\AppData\Local" there's a Tecnomatix folder which contains some user xml config. This folder is automatically created when starting TX and keeps being updated as you change software config.

 

Try to rename/delete this folder and start the software again. I experienced in the past some issues related with this folder.

 

Regards,

 

 

 

Re: PS Application Starting then Immediately shuts down

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Check if you can run PS/PD via Desktop Icon with graphic processor

  1. Right mouse click on desktop icon
  2. Run with graphic processor
  3. NVIDIA Processor (Standard)

 

Or...

 

When using NVIDIA graphics...

  1. Open Nividia Control Panel. (right mouse click on Desktop)
  2. In tree select "manage 3D settings".
  3. "Select program settings" tab.
  4. Search for "Siemens Teamcenter (Siemens Teamcenter Tune) process.
  5. In the list below scroll down to "Threated Optimization".
    Switch "OFF".

You can also switch "off" the internal "Intel" graphic chip in BIOS.

 

 

Best regards

Patrick