Cancel
Showing results for 
Search instead for 
Did you mean: 

PS - OLP commands for key signals?

Pioneer
Pioneer

Hi all,

 

When starting up a line simulation I often end up in a catch-22 situation.

 

Scenario: Robot 1 delivers a part to Robot 2.

 

In order for Robot 1 to get an enable signal (to avoid collisions etc.), Robot 2 must send an enable signal to Robot 1. But since Robot 2 hasn't completed its first cycle yet it has no enable signal to send.

 

I could split the operation of Robot 1 and use transition conditions instead, but in my opinion that seems like a bad solution since I would end up with a large number of smaller operations. That's why I would prefer to use OLP commands.

 

I wish the OLP command for the Robot 1 wait location could look something like this:

 

# WaitSignal  IN_ROBOT1 1 OR NOT "SIGNAL_EVENT_WHEN_ROBOT2_STARTS"

 

Is it possible to set/wait for key signals using OLP commands or is there another solution?

6 REPLIES

Re: PS - OLP commands for key signals?

Siemens Phenom Siemens Phenom
Siemens Phenom

You can manually write:

# WaitSignals <any robot signal expression>

Note the 's' in WaitSignals.

Only robot signals of the given robot can be tested, so you have to properly map your signal connections via logic blocks.

Re: PS - OLP commands for key signals?

Pioneer
Pioneer

I'm not sure how to write the expression syntax with an "OR" statement. Is this even remotely correct?

 

# WaitSignals Robot1_EndSignal_IN_Robot2 1 OR Robot1_StartSignal_IN_Robot2 0

 

Robot1_EndSignal_IN_Robot2 = Robot2's enable signal at Robot2 cycle end

Robot1_StartSignal_IN_Robot2 = Robot2's signal at Robot2 cycle start

 

 

I have mapped the I/O:s in the Module Editor.

 

When running the simulation I receive this error: "Failed to extract signals from expression 'Robot1_EndSignal_IN_ROBOT2 1 OR Robot1_StartSignal_IN_Robot2 0'".

Re: PS - OLP commands for key signals?

Siemens Phenom Siemens Phenom
Siemens Phenom

# WaitSignals (Robot1_EndSignal_IN_Robot2 == 1) OR (Robot1_StartSignal_IN_Robot2 == 0)

You can also use AND, XOR, >, <, etc...

Re: PS - OLP commands for key signals?

Pioneer
Pioneer

Thanks for your help!

 

Now I receive a new error:

 

"Signal Robot1_EndSignal_IN_Robot2 not found, value 0 is assumed"
"Signal Robot1_StartSignal_IN_Robot2 not found, value 0 is assumed"

 

The signals are working in the Simulation Panel.

Re: PS - OLP commands for key signals?

Siemens Phenom Siemens Phenom
Siemens Phenom

In the OLP Command you need to use the "Robot Signal name", not the "PLC Signal name" that you can see in the Simulation Panel.

Re: PS - OLP commands for key signals?

Pioneer
Pioneer

Of course! Now it's working.

 

Thank you so much!