Showing results for 
Search instead for 
Did you mean: 

[PS11.1] Posenames with spaces are problematic




it is possible to give poses  a name containing space characters.

But if you want to use this posename in a Drive device command it does not work. No error message will pop up as well!

Drive Device does not accept space characters.

Is this a known problem?



Re: [PS11.1] Posenames with spaces are problematic

Siemens Phenom Siemens Phenom
Siemens Phenom



Tested in PS13.1 and there is the same behavior.

The best will be to report this issue to GTAC.



Best regards


Re: [PS11.1] Posenames with spaces are problematic

Valued Contributor
Valued Contributor

Not only here. all object name with space in between will be in trouble while it is save to cojt.

this is pretty often happened while you load a jt file and set its kinematics attribute and save back to eMserver.

So please make sure that There is no space between name characters. using _ to connect them Cat Happy