Cancel
Showing results for 
Search instead for 
Did you mean: 

[PS11.1] System error code -2118952392

Legend
Legend

Hello,

if I try to rename nodes in the object tree, I often get the MessageBox(of death)

Fatal error: Unknown reason (System error code: -2118952392) Saving dump file ...

 

Can someone tell me what causes this error and how I can avoid it?

1 REPLY 1

Re: [PS11.1] System error code -2118952392

Siemens Phenom Siemens Phenom
Siemens Phenom

This is almost impossible to track down, when it's not reproducable.

 

As dump file creation is obviously enabled, you may also enable the dump-file diagnostic tool in eMPowerDoctor.

It will write a log-table, that keeps info about each crash.

You may then open an IR in GTAC and upload your dump-file.

Maybe it will tell the cause of the crash.