Cancel
Showing results for 
Search instead for 
Did you mean: 

[PS11.1] Transfer operations to another study with default controller

Legend
Legend

Hi all!

 

Is it possible to transfer operations from one study to another study with the default controller?

Similar to the "Store path - Load path" function in Robcad.

 

3 REPLIES 3

Re: [PS11.1] Transfer operations to another study with default controller

Siemens Phenom Siemens Phenom
Siemens Phenom

Not that I know. A workaround would be to create a XML Motion Customization that generates a format compatible with "Upload Robcad Robotic Programs".

Re: [PS11.1] Transfer operations to another study with default controller

Legend
Legend
Thank you very much for the answer!
But is there a particular reason why uploading default robot programs is not supported.

Re: [PS11.1] Transfer operations to another study with default controller

Siemens Phenom Siemens Phenom
Siemens Phenom

There was no real demand for it. If you use a real controller, you can transfer by download + upload (that also can be a workaround).