Cancel
Showing results for 
Search instead for 
Did you mean: 

Path Template XML element for "Gun Wait"

Pioneer
Pioneer

I use KUKA controller in PS and I need to set status "No Wait" for the gun when applying custom path template.

 

1.png

 

What text should I place in custom XMLs in PathTemplateConfiguration and in MotionConfiguration folders?

 

1 REPLY

Re: Path Template XML element for "Gun Wait"

Gears Phenom Gears Phenom
Gears Phenom

have you check this parameter?

 

pointed to by RefLoc.
<Action Name="AddApproachLocation" LocRange="First">
<AddLoc Name="approachViaLoc" RefLoc=" First " Placed="After" CopyAttachment ="true" RelX="-100.05" RelZ="100.05">
<!--apply to the added via location only-->
<Param Name="Gun Wait" Dynamic="true" Value="No Wait"/>
</AddLoc>
<!--apply to the output of the filter-->
<Param Name="RRS_MOTION_TYPE" Value="2"/>
</Action>

Kind regards,

Benjamin Voelzke