Cancel
Showing results for 
Search instead for 
Did you mean: 

Possibility Virtual Commissioning using multiple PLC'S in Process Simulate

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

 

Dear Experts,

 

One of our customer is interested in simulating entire line in process simulate using multiple PLC’S.

 

Currently they are using Kepware OPC server, S7 1200 PLC and PS 13.1.

 

Is it possible to connect Multiple PLC’S to Kepware and simulate entire line in PS?

If yes what is the maximum limit?

 

Thanks in Advance

Jeethan Rohan  

Best Regards,
Jeethan Rohan
2 REPLIES 2

Re: Possibility Virtual Commissioning using multiple PLC'S in Process Simulate

Siemens Legend Siemens Legend
Siemens Legend

Hi

 

If your'e asking about limiations of the Kepware OPC server, I suggest you visit KepWare forums which can better supply an answer. 

 

For Process Simulate you can define any number of parallel "External Connections" and assign differnt signals to different connections so you could connect to several different KepWare OPC servers in parallel. 

I do not think there's a limit to how many external connections can be used in parallel. 

Kind regards,
Gal Snir

Re: Possibility Virtual Commissioning using multiple PLC'S in Process Simulate

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Hi,

Thanks for the information, I will check in the KepWare forums.
Best Regards,
Jeethan Rohan