Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with applying path template

Creator
Creator

Hi,

 

I was following the following tutorial: https://www.youtube.com/watch?v=Y3Uq2cee8pU&index=5&list=PL1m1vu8_quoCkCBRbz6OhfiRy0sL66jvW#t=15.805...

 

I'm using RobotExpert 12.1.3.

 

When trying to do as the example, there are two issues:

1. Where is the PathTemplateConfiguration - folder?

2. How can I fix the error message in the picture?2016-04-19_17-51-00.png

3 REPLIES

Re: Problem with applying path template

Creator
Creator
Fixed this by installing the default robot controller from the download section.

Re: Problem with applying path template

Siemens Legend Siemens Legend
Siemens Legend

The templates are located under Tecnomatix installation folder/eMPower/Robotics/Olp/<controller name>/PathTemplateConfiguration.

 

The error message can be fixed by removing the error in the template.

CustomizeXmlChecker command (you will need to add that command to the ribbon or use the find command) will provide you with all debugging information to help you finding and fixing the error.

 

 

Re: Problem with applying path template

Pioneer
Pioneer

Hello    lagi

can you download the Youtube video and then send it to my E-mailbox  gangw815@163.com?

i can not browse the Youtube video.

 

thanks very much.

 

best wishes

wang gang