Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with Object Flow Operations after saving

Experimenter
Experimenter

Hello,

 

i got a problem with some Object Flow Operations after saving and restart the project.

 

My Object Flow Operation:

Forum Siemens.PNG

When i created the Object Flow Operation it worked fine  http://imgur.com/a/4R1h1. Than i saved the project, next day i wanted to continue my work but this happend with some of my operations:

 

Forum Siemens2.PNG

 

Some of my parts moved to the right, i dont know why.

What i did up to now:

-delete the broken operations and insert new ones -> Saving+Restart = Same problem

-checking all the path if there is a error -> nothing found

 

Does anybody know this problem? I don´t know what to do

 

Thanks & Greetings

 

Chris

 

 

3 REPLIES

Re: Problems with Object Flow Operations after saving

Siemens Legend Siemens Legend
Siemens Legend

Hello Chris,

 

when you create the object flow operation, the system creates a grip frame (by default located at the part geometric center). The frame should exist in the frame section of object tree, named <operation>_grip, attached to the part

 

when playing the operation, that grip frame should move along the path.

 

check if this frame exists and if its relative position to the part has not changed.

 

Best regards

Bernard

 

Re: Problems with Object Flow Operations after saving

Genius
Genius

Bernard's comment is exactly rightSmiley Happy

 

One tip here:

 

using snapshot function to 'remember' your initial postion of product or resources. one they fly over to somewhere else. just click remembered snapshot. it will restore its postion... very handy.

 

this function existed in snapshot view.

 

Enjoy.

Steven

Re: Problems with Object Flow Operations after saving

Experimenter
Experimenter

Hello,

 

the frame "<operation>_grip" is existing and the its relative position to the part has not changed.

 

I fixed the problem. After lot of trys I noticed that the problem only exist in my "master" compound operation.

My project structure looks like this:

  • Master Compound OP
    • Compound OP 1
      • Objectflow Operations
      • < >Operations
    • Compound OP 2
    • Compound OP n ...

When I was modeling the operations I only worked in my Master Compound. When I simulate the Master Compound OP I got the problem. But if I set the Compound OP with the problem as current and simulate it the problem disappeared. After the the simulation in the Compound OP I can set the Master Compound OP as current back and the problem here also disappeard. I don´t know why, but its works Smiley Happy

 

 

Thank (Danke) for your help!!

 

Greets

 

Chris