Cancel
Showing results for 
Search instead for 
Did you mean: 

Process Simulate 11.1 TR01 Standalone Version

Gears Phenom Gears Phenom
Gears Phenom

 

I have a question about the process simulate standalone version.
 
In the product information will be so advertised, that can make you can also line simulation (CEE).
 
Unfortunately, I can create no twin objects in a new cell. With the correct structure, I can switch in the line mode.
 
Admin Console is not available.
 
Is it possible the CEE mode in the standalone version to use?
 
Kind regards,

Benjamin Voelzke
4 REPLIES

Re: Process Simulate 11.1 TR01 Standalone Version

Siemens Genius Siemens Genius
Siemens Genius

You are partially correct.

If you start a totally new study in disconnected, then you cannot create a twin object (PrStationProcess) and thus cannot run event based simulations.

If you get a study that already has this twin - you can.

We are working to fix this gap and will hopefully support all use cases soon.

Regards,

Gil Chen.

Re: Process Simulate 11.1 TR01 Standalone Version

Gears Phenom Gears Phenom
Gears Phenom

thanks.

Kind regards,

Benjamin Voelzke

Re: Process Simulate 11.1 TR01 Standalone Version

Experimenter
Experimenter

Hello,

 

I have the same problem with the standalone version. Is there already a solution? This post is from more than a year ago.

Re: Process Simulate 11.1 TR01 Standalone Version

Siemens Legend Siemens Legend
Siemens Legend

Hello

 

Yes - this issue was resolved in TMX  11.1.TR3

You still cannot create twin objects in PS Standalone, but for Line Simulation mode you no longer have to use them as well - you can use any Compound Operation instead.

 

In any study - move all your operations under Compound Operations, and than save and Switch\Open to LS mode. 

 

 

 

 

Kind regards,
Gal Snir