Cancel
Showing results for 
Search instead for 
Did you mean: 

Process Simulate 13: Lost tool mount information after study reload

Experimenter
Experimenter

Hi everybody,

 

it happens not usually. But sometimes, when iam loading my study, all my mounted tools are gone. I mount the tools a second time, so i can simulate, but the time i put into this extra work, is gone.


How can i avoid this?

 

Thanks for reading

 

Kind regards 

9 REPLIES

Re: Process Simulate 13: Lost tool mount information after study reload

Creator
Creator

When you are saying they are "gone", do you mean the tools are dismounted for no reason or removed from the study (as in no longer appearing in the object tree) ?

Re: Process Simulate 13: Lost tool mount information after study reload

Experimenter
Experimenter

Yes, they are dismounted for no reason. 

 

I mount them again.

 

When iam finished my work for the day: Save study,close Simulate.

 

Next day: Open Simulate, open study and the tools are not mounted.

 

 

Re: Process Simulate 13: Lost tool mount information after study reload

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

do you work in standard mode or in Line simulation mode?

 

on with frame do you mountet?

 

Do you mountet the tools via OLP logic or direct by function`?

 

thanks

Kind regards,

Benjamin Voelzke

Re: Process Simulate 13: Lost tool mount information after study reload

Experimenter
Experimenter

Iam working in Standard Mode and i mount the tool with toolframe on robotframe axis 6. 

 

We use the robot tool box to mount tools. Add tool, define TCP, physical on TCP Frame. 

 

When i attach the tools on the robot, without Mounting or with Mounting, its the same problem.

 

After loading the study, the tool have no connections with the robot.

 

First thing i do every new day, is to mount my tools. 

Re: Process Simulate 13: Lost tool mount information after study reload

Siemens Phenom Siemens Phenom
Siemens Phenom
Obviously this is no normal behavior.

I believe your study is corrupted.
In order to check your data, I recommend to contact GTAC and provide the data.

Before that, you should investigate a few things, like:
- does the same happen in a new study
- do common attachment work at all
- is other study information stored at all (notes, colors, frames)

Re: Process Simulate 13: Lost tool mount information after study reload

Experimenter
Experimenter

We create the study with Process Simulate Version 11 and change to Version 13 during project. 

 

But new stuys, create with Version 13 and never be in contact with Version 11, have the same issue. 

 

I thought, it might be a config failure. 

Re: Process Simulate 13: Lost tool mount information after study reload

Siemens Phenom Siemens Phenom
Siemens Phenom
Are you working on TC?
Maybe missing write access to your study?
Check if your study object has only one dataset of a kind. Sometimes it behaves a bit strange.

Did you check other study info, mentioned in my previous post?

Re: Process Simulate 13: Lost tool mount information after study reload

Experimenter
Experimenter

Yes, my cable assembly are still attached. Colours are still there, Notes are ok.

 

Hmmm. I create a new study and test again. 

 

Thanks for your advice! Smiley Wink

Re: Process Simulate 13: Lost tool mount information after study reload

Creator
Creator

Please check Tune cell data.? When you moved from PS 11 to PS 13 have you copied all Tune cell data ?

Most of the time it is related with Tune cells only.