07-22-2016 09:43 AM - edited 07-22-2016 09:50 AM
Hi guys,
I work for a short time with Process Simulate and need your help.
I have two robots that collide during simulation. So I want to set one to make a break, until the second leaves the zone where they could meet (Interference Volume or zone).
This must be controlled by “logic block”, right?
I would be very happy if anyone can help me and explain the procedure for a beginner.
My problem is that I don´t know how I can enter this in Logic Block.
Thank you in advance
07-26-2016 08:55 AM
Hi,
actually this is a typical question that is answered in a training.
But also in the manual.
You CAN solve this by LogicBlock.
But it's even more simple using a module >> "Modules Viewer"
1. Add relevant robot-signals that handle the zone-request
2. create a Module
3. edit and add the necessary expression and resulting robot-signal
4. pull the module down into the hierarchy under "OB1"
That's it.
06-09-2017 06:51 AM - edited 06-09-2017 06:53 AM
Can I use "Interference Zone" command to specify zones where a collision can take place?
Or what workflow do you suggest?
06-18-2017 03:54 AM
You can use the "Automatic Interference" command to create:
1. Swept Volumes of the robotics operations
2. Interference Volume out of the Swept Volumes
3. Most importantly the command will create OLP comments on locations which are right before\after the robot entering the interfernce volume (e.g. "Last location before <Robot name> enters <Volume name>").
You can then replace these commands manually with you required instructions for the robot (Set Signal, Wait Signals, etc.) or by creating a Path Template you can apply.
4. The two robots will both talk to your LB/Module which will handle the communication between them.
06-19-2017 02:23 AM - edited 06-19-2017 02:24 AM
Thank you. I just find out this commands (Set Signal, Wait Signals) and it works great!
10-25-2018 01:07 PM
Hello,
Can you please post a screenshot of an example showing the module for the interference signals? I'm trying to establish an interference zone between two colliding robots but I donot know how to do that exactly.
Thank you for your time.
12-26-2018 04:01 PM
Hello
Well - the logic really depends on your real logic.
There are many ways to achieve this and you should strive to model the logic after the real robot's logic.
You only have to model such an LB once (and can make it adapatable to more robots for example) and then can reuse it over and over.
In general the return from your module\LB\PLC should take into account at the very least the request itself and the not-occuipied signal of the requested zone. Possible also to make sure requests from other robots are not coming in and more...
Watch Replays of Previous Topics