Cancel
Showing results for 
Search instead for 
Did you mean: 

Process Simulate Movie Capture closer to real time?

Genius
Genius

Hi,

is there anyone that has some tips on how to create a movie out from Process Simualte where the movie length corresponds to the rcs simulated time?

This is of course not always good but sometimes it is beneficial to show the movie in "real time".

In the old Robcad days you could set the update rate to about 0.04s which would give something a bit closer to real time but that is not really good enough.

Any tips on how to achieve this would be higly appreciated!

 

 

Kind Regards

Andreas

3 REPLIES 3

Re: Process Simulate Movie Capture closer to real time?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi, the only option I know, is to set Simulation time to real time 1:1 ration. This feature is available since version 12.1. However, it's usefull only when the simulation runs faster than in real.

 

D.

Re: Process Simulate Movie Capture closer to real time?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi ajonss32 and Dave007,

please check this post.

It will provide both MovieCapturing and add realtime-button the earlies versions.

Regards,

Guido

Re: Process Simulate Movie Capture closer to real time?

Genius
Genius

Hi Guido,

perfect, thank you! Your solution also improves both performance and most of all the overall size of the movies which is great.

 

Once again, thank you!

 

Kind Regards

Andreas