Cancel
Showing results for 
Search instead for 
Did you mean: 

Query regarding insertion of robot

Creator
Creator

Hello All,

 

I had .co robocad file of robot model, which I converted into .cojt file using

Program Files\Tecnomatix_13.0.2\eMPower\UpgradeToVersionWin.exe.

 

After successfully converting into .cojt format, the same file was imported into PS environment using Import/Export-Convert and Insert CAD files.

 

After coverting, the window displays, "The conversion completed successfully, but the JT file isn't an assembly one", and the model is not displaying in the window.

 

Could anyone please address this query.

 

Thanks and Regards,

Sriram

2 REPLIES

Re: Query regarding insertion of robot

Valued Contributor
Valued Contributor

It looks you are running a wrong working way here...

robcad .co file updates to .cojt file--> correct.

then

you need to set this .cojt file to a resource prototype in Process Simulate ( create a library component). then load it into your PS. ( select it from library and insert into your cell/zone/area...).

this working way is classic and should be no problem.

 

Just try it...

Re: Query regarding insertion of robot

Creator
Creator

Thank you Steven for your reply.

 

Since, I am new to PS, I could not find resource prototype (create a library component) in PS environment.

 

Can you suggest pathway for resource prototype in PS environment.

 

Thanks and Regards,

Sriram C S