Cancel
Showing results for 
Search instead for 
Did you mean: 

RCS ABB rw6.05.02

Experimenter
Experimenter

Hi, Is there any reason why ABB rw6.05.02 RCS is not available on the GTAC download server? Thanks

3 REPLIES 3

Re: RCS ABB rw6.05.02

Siemens Phenom Siemens Phenom
Siemens Phenom

We never received this version from ABB.

Re: RCS ABB rw6.05.02

Experimenter
Experimenter

I guess that makes sense, thanks GillesVelay 

 

The reason why I ask is the ABB robots we are working with on a particular site I believe are running rw06.05.02. Do you know what kind of an impact using rw06.05.03 in Process Simulate would have on the paths, motion, config etc.?

 

Thanks again

Re: RCS ABB rw6.05.02

Siemens Phenom Siemens Phenom
Siemens Phenom

I would compare the cycle time on a meaningful path between 06.05.01 abd 06.05.03. If you get the same, as I assume, then you can assume 06.05.02 would behave like those 2.

ABB usually do not provide the details of the changes between minor releases.

 

If you have difference, then we can contact ABB to get a RCS for 06.05.02.