Cancel
Showing results for 
Search instead for 
Did you mean: 

ROBOTEXPERT ArcCell Open Error - Free Trial Version

Legend
Legend

Hi all,

 

I am a user of teconmatix plant simulation.

As we plan to run the Fanuc robots running in the real installation also in our model, I loaded RobotExpert.

I have installed the free trial version of the RobotExpert software.

There is one example included: ArcCell Welding.

A list of error show up when I try to open it.

 

Did anybody have a similar issue ?

 

Kind regards

Marco

 

8 REPLIES 8

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Siemens Phenom Siemens Phenom
Siemens Phenom

Most probaly you did not set the library-root. So Robot Expert does not know where in your file-system your components are.

Currently your root is set to c:\temp.

 

Did you follow the "Getting Started" tutorial movies? (should be in your installation folder under  Tecnomatix\Tutorials\GettingStarted)

First movie 1._Graphic_Manipulation.mp4 shows how to set the library properly at the beginning.

 

 

 

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Legend
Legend

Hi Guido,

 

I have updated the Library path in the 'Options', but it does not make any difference.

 

 

 

 

Kind regards

Marco

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Legend
Legend

Hi Guido,

 

I added a screen shotof the path.

I have updated the Library path in the 'Options', but it does not make any difference.

  

The errors are still:

Errors:

The following components are not defined as devices:
Name = DK-250H 143945_step  ID = Id#3386AAD6-1D97-47AA-BA45-552F321099C8
Name = ma01800_a00  ID = Id#C8F21F49-6B35-4406-B734-6D6EA45D23BD
Name = '''Robacta5000_36_S_type'  ID = Id#8527B4CE-3E78-4292-9AA8-81694A29CE76
Name = DK-250H 143945_step  ID = Id#3386AAD6-1D97-47AA-BA45-552F321099C8

.... and the warnings, but I don't think this matters, I hope.

 

Kind regards

Marco

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Marco,

again: pls follow the "getting started"-guide.

It tells to set the path to "ArcWeld_Library", not to "libraries".

Go one folder up.

 

Each device/robot/part in the study is stored with it's relative path, starting from that folder.

The path of the library must be 100% correct.

 

2018-01-11 09_17_59-1._Graphic_Manipulation.mp4.png

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Legend
Legend

Hi Guido,

 

yes, you are right, sorry.

Now the model can be opened.

 

 

Kind regards

Marco

 

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Experimenter
Experimenter
hello sir can you help me ? i downloaded robot expert free trial and when i try to open example included (ArcCell) it oprns but don't open the cell this is a screen of what appears
 

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Legend
Legend

Sorry, but I can't help you. I have never used the robot expert software.

Last year as I was at the early stage of including robots into the plant sim, I downloaded this package.

But I never used it. This project was suspended as I started to work on another model.

I think Guido should the right person to help you.

 

Regards

 

Re: ROBOTEXPERT ArcCell Open Error - Free Trial Version

Experimenter
Experimenter

ok thanks