Showing results for 
Search instead for 
Did you mean: 

Relocate an appearance?

Valued Contributor
Valued Contributor

Hi all!


I have assigned a part to an operation. When I switch to line sim mode en run the operation the part appears in a different position then when I run the operation in a time-bases sim. I can use the relocate option, but why does the position change? Is there a way to set the initial postion?


Best Regards.




Re: Relocate an appearance?

Siemens Phenom Siemens Phenom
Siemens Phenom
The position of the appearance is stored on the generating operation.
Just ‎do

* generate appearance on your operation
* relocate appearance to desired position
* delete the appearance
* store the study

Siemens Industry Software GmbH & Co. KG; Anschrift: Franz-Geuer-Str. 10, 50823 Köln;
Kommanditgesellschaft: Sitz der Gesellschaft: Köln; Registergericht: Amtsgericht Köln, HRA 28227;
Geschäftsführung und persönlich haftender Gesellschafter: Siemens Industry Software Management GmbH;
Geschäftsführer: Urban August, Daniel Trebes; Sitz der Gesellschaft: Köln; Registergericht: Amtsgericht Köln, HRB 70858