Cancel
Showing results for 
Search instead for 
Did you mean: 

Robcad abb robot to process simulate

Experimenter
Experimenter

Hi!

 

I'm a new user of process simulate and have the following question. I downloaded a robot model from ABB's webpage in Robcad format. I want to import this model inte PS and tried the "Upgrade CO to version" but I couldn't get it to work. Nothing at all happened when I used the software, no changes to the .CO file, no JT-file or log-file was created. Can someone please give me some instructions how to proceed!!!!

 

 

18 REPLIES 18

Re: Robcad abb robot to process simulate

Siemens Legend Siemens Legend
Siemens Legend

It is likely that this robot model is a Robcad Supercomponent (i.e. includes sub components). in this case you need to have all subcomponents and set properly the library root in the upgradeToComponent dialog.

Re: Robcad abb robot to process simulate

Experimenter
Experimenter

Hi!

 

Thanks!

But I still have the same problem, nothing happens. If someone have the time to test, I attach the robcad file and the "Upgrade CO to Version" dialog with the settings I used.

 

Cheers!

 

Re: Robcad abb robot to process simulate

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

this is not a supercomponent. I think the problem is that you did not install CAD Setup and you are missing some software elements.

Re: Robcad abb robot to process simulate

Experimenter
Experimenter

Thanks again!

 

Is it possible for you to be more specific? I have installed the CAD-translators from CD2, is there something more that has be there to get it work?

Re: Robcad abb robot to process simulate

Siemens Legend Siemens Legend
Siemens Legend

this is very strange. Do you have upgradetoversion.exe in the eMPower folder? tyou can run the conversion as command line.

 

In any case, that component converts properly, the result is attached

Re: Robcad abb robot to process simulate

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Try to use command line version directly:

 

syntax:

 

upgradetoversion -comp "full path to your .co" -co2jt

 

for example:

 

upgradetoversion -comp "D:\technomatix\Robot_models\ABB\irb6_5.co" -co2jt

Re: Robcad abb robot to process simulate

Experimenter
Experimenter

I tried this method as well with the same results

Re: Robcad abb robot to process simulate

Siemens Legend Siemens Legend
Siemens Legend

HI,

 

something is definitely wrong in your installation. Please contact GTAC to get that fixed

Re: Robcad abb robot to process simulate

Legend
Legend

Hi,

 

I think you robot in .co file is an older robcad model.
Unfortunately, there is no .info file included in the .co.

But I think it is an older model.

In this case you need to upgrade to component first.

The command is upgrade_to_version -comp >> this is only available if Robcad is installed on your machine.