Cancel
Showing results for 
Search instead for 
Did you mean: 

Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I have install all hotfixes from PS11.1 on my Robot Expert 11.1 version.

 

Robot Toolbox is working after the hotfix update but ignore logic dosen't work with fanuc robots.

Is this sure???

 

 

 

 

 

Kind regards,

Benjamin Voelzke
8 REPLIES 8

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

Siemens Legend Siemens Legend
Siemens Legend

Hi Benjamin.

Do you mean to say the feature is not added to RE after installing the HFX ? Or that it doesn't work ?

 

If it's the former, did you install HFX01 ?

We discussed this issue in a previous post ("Robot Expert V11.1 missing function (ignore OLP signals)" and at the time I installed RE11.1 with HFX 01 and had the feature avaialble to me.

 

If it's the later - what OLP commands are not skipped ?

Kind regards,
Gal Snir

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

today i have install RE 11.1 TR01.

In Version 11.1 with HF and 11.1 TR01 is the new button (ignore OLP ) avialable.

 

But the function dosen't work correctly.

See screenshots.

 

under options i activate the function but thr robot waits for input signals.

 

2014-05-19 13_09_46-Options.jpg2014-05-19 13_10_01-.jpg

Kind regards,

Benjamin Voelzke

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

Siemens Phenom Siemens Phenom
Siemens Phenom

Ignore Logics has a different purpose from Ignore Signals...

 

There is no "Ignore Signals" option available in Robot Expert yet.

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

how can i simulate a real robot path in Robot Expert?

 

today the path is not running! (allways wait for Inputs)

 

Force Signals is not available in RE!!!

 

i can only jump to the positions.

 

 

Kind regards,

Benjamin Voelzke

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

Siemens Phenom Siemens Phenom
Siemens Phenom

There is ER1952414 to have "Ignore Signals" in Robot Expert...

 

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

Siemens Phenom Siemens Phenom
Siemens Phenom

In next controller versions on Robot Expert, signals will be automatically ignored when the operation is simulated from the Path Editor. They will not be automatically ignored if the operation(s) is/are run from the Sequence Editor.

This way, until the above mentioned ER is implemented, it will be possible to run operations that contain signal commands by ignoring them (Path Editor should be used) while still possible to simulate "ToRobot" signal exchanges (Sequence Editor should be used).

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

ignore signals in path editor is ok.

but in sequence editor i will simulate with signals and without signals. (depents on use case)

 

thanks

Kind regards,

Benjamin Voelzke

Re: Robot Expert 11.1 ignore OLP logic dosen't work with Fanuc Robots

Siemens Phenom Siemens Phenom
Siemens Phenom

In sequence editor, behavior will be linked to the (future) "Ignore Signals" setting, so you will be able to ignore signals or not. In the current version, signals will never be ignored in sequence editor (and always in path editor).