Cancel
Showing results for 
Search instead for 
Did you mean: 

Robot Expert: Using a CLSF file from NX CAM

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

What is the correct application to add to Robot Expert to allow for cls input?  I have downloaded and installed RobotExpert_11.1 TR2_NC_CODE_64BIT_v1.10.1_26_05_2014.exe.  I see nothing different in the interface. 

 

Are there any sample files for Robot Expert that already include all of the objects required for simulation?  I'm having trouble understanding the basic workflow of the application.

 

I am trying to simulate a surgical procedure, where a Kuka robot is used to prepare a femur for a prosthetic implant.  I have used NX CAM extensively, but am new to Robot Expert.

1 REPLY

Re: Robot Expert: Using a CLSF file from NX CAM

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

The application to add is RobotExpert_11.1TR2_CLS_UPLOAD_64BIT_v1.4.6_03_07_2014.exe NEW!  or similiar.  Once installed, add it to your customization.  Create a cell using the same Kuka robot model and import a CLSF from NX that matches your implant.