Cancel
Showing results for 
Search instead for 
Did you mean: 

Robot Expert V11.1 missing function (ignore OLP signals)

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

hello,

 

i have tested robot expert v11.1

 

i miss the function "ignore OLP Logic" from the newest Hotfix of process simulate.

 

can you implement this function in robot expert,please ?

 

thanks

 

4 REPLIES

Re: Robot Expert V11.1 missing function (ignore OLP signals)

Gears Phenom Gears Phenom
Gears Phenom

Is this function inplemented in version 11.1 TR02?

 

Kind regards,

Benjamin Voelzke

Re: Robot Expert V11.1 missing function (ignore OLP signals)

Siemens Legend Siemens Legend
Siemens Legend

Hi.

This function is implemented in V11.1TR1 and is also included in HFX 01 for V11.1 (meaning 111hotfix00-01, not the latest one), so you need to install this HFX from the FTP to get the feature.

 

There's also a HFX for v10.1.

 

Let me know if this works,  

 

 

Kind regards,
Gal Snir

Re: Robot Expert V11.1 missing function (ignore OLP signals)

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

can I install the same patch for "Robot Expert", such as for process simulate?

 

There are no "robot expert" patch on the FTP server.

Re: Robot Expert V11.1 missing function (ignore OLP signals)

Siemens Legend Siemens Legend
Siemens Legend

Hello.

Up to v11.x there was a seperate category for HFX for Robot  Expert. You can find it on the website in a different folder (HFX for PS are under tecnomatix->Planning_Applications while HFX for Robot Expert are under tecnoamtix->Robot Expert).

Since v11.1.x and afterwards the HFX were merged so installing the same HFX will work for both Process Simulate and Robot Expert (assuming the HFX is valid for RE).

 

I've installed RE11.1 and HFX 01 and this specific HFX (Ignore OLP Logic) is indeed implemented:

RE_HFX.jpg

 

Kind regards,
Gal Snir