Cancel
Showing results for 
Search instead for 
Did you mean: 

Robot limitation with ABB rcs?

Valued Contributor
Valued Contributor

God morning guys,

 

at the moment I am working with PS 10.1, rcsabb_rw5.15.05.irc5.

When I try to start a simulation with more the four robots, I get following error message on the fifth robot:

 

------------------------------------------

ir_110060r03[RRS]> Hinweis an (p_40_v60w32_rx32) ToolHome1: RRS Meldung: ERROR:

50290: Service unavailable

Unable to obtain correct license.

 

Please check the license settings.

ir_110060r03[RRS]> Fehler an (p_40_v60w32_rx32) ToolHome1: Bewegung gescheitert: Internal software error., Fehler Code: -49

------------------------------------------

 

My flexlm-diagnostics says_

 

------------------------------------------

"abb_getnextstep" v5.0, vendor: rcsablmd
  License server: xbz
  floating license no expiration date

------------------------------------------

 

Is this a bug or just a licence limitation?

Thanks for your help Smiley Happy

 

 

 

2 REPLIES

Re: Robot limitation with ABB rcs?

Siemens Phenom Siemens Phenom
Siemens Phenom

Most probably a license limitation. Look at your license file:

 

Ex:

 

FEATURE abb_getnextstep rcsablmd 1.0 31-jan-2014 10 SIGN=65A8368474FA

 

The value 10 over there tells you that you can concurrently run up to 10 robots. You probably have 4.

Re: Robot limitation with ABB rcs?

Valued Contributor
Valued Contributor
Thats correct -thank you!