Cancel
Showing results for 
Search instead for 
Did you mean: 

RobotExpert Apply path template error

Hello everyone,

 

am getting an error in RobotExpert 12.1 while accessing Apply path template from Path Editing option.

 

have attached the steps that i have followed in the ppt.

 

Request to provide a suitable solution ASAP.

 

2 REPLIES 2

Re: RobotExpert Apply path template error

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

hello,

 

you load the demo cell without controller. "default"

If you change the robot controller to abb you can see the problem in the background with xmls.

 

RE and PS have problems after change the robot controller to "default" in Background search RE and PS the old syntax.

 

please check the robotsmachinedatafiles folder.

do you have in these folder wrong files RE check these.

Kind regards,

Benjamin Voelzke

Re: RobotExpert Apply path template error

Thanks for your reply voelzke,

 

have checked these options. Actually there was an xml file missing which contained the data required in folders like OLPCinfiguration, DataConfiguration in the respective controllers installed.

 

Now have done an xml customization and errors are gone.

 

Some Actions, params were to be incorporated. Have done it and its working fine now.

 

Thank you.