Cancel
Showing results for 
Search instead for 
Did you mean: 

Running Line simulation with Simulation unit(simba unit)

Valued Contributor
Valued Contributor

Hi

 

I have setup a cell using a simulation unit(9AE4120-2AB00: SIMULATION UNIT PN256) and software SIMULATIONUnit_V8.3 all on process simulation 13.0

 

I have setup everything and I tested the signal by forcing it true in the simulation unit software and it goes throught to the PLC(SIMATIC S7-1518-F ) all looks good. But now as soon as I add just this signal to the simulation panel and hit the play button in process simulation and force the signal to true it starts flashing on and off with no other logic blocks running.

 

I have tested this signal with a totally random signal that is not used anywhere on the PLC code but still this issue occurs.

 

Does anybody have anyidea why this could occur and how to fix it

 

Thanks

          

4 REPLIES 4

Re: Running Line simulation with Simulation unit(simba unit)

Siemens Legend Siemens Legend
Siemens Legend

Hi RobSimCoder

 

Well - this sounds like there's a conflict on the Signal's value. I understand there are no LB's triggering this signal (did you run a Cross Reference check on it to make sure no one else is handling it?), but perhaps other parts of your PLC code are still refering to it? Is the signal state flashing also on the PLC side?

 

 

 

Kind regards,
Gal Snir

Re: Running Line simulation with Simulation unit(simba unit)

Valued Contributor
Valued Contributor

Hi

 

If I restart my process simulation machine the problem go away for a while and then comes back at a unknow time. So it cannot be logic causing it

 

Thanks

Re: Running Line simulation with Simulation unit(simba unit)

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

flashing signals I also experienced some time ago.

In my setup it was caused by the switch that we used.

The expensive, configurable high-end GBit switch caused the problem.

A 10€ switch from the discounter worked without problems.

 

Also: are you sure Simba-sides (PLC&Simulation) are not configured in the same IP-network?

Re: Running Line simulation with Simulation unit(simba unit)

Valued Contributor
Valued Contributor

Hi

 

Hmm yes thank you I will test this as it sound like a probable cause.

 

Thanks