Cancel
Showing results for 
Search instead for 
Did you mean: 

Seeking a solution for the automatic connection mapping function.

Gears Phenom Gears Phenom
Gears Phenom

good day,

Seeking a solution for the automatic connection mapping function.
currently I can only connect signals with resources that are available in the study.

My wish
The connection to the resource mapping function / logic blocks from the Library then drag copy the cell and rename according to handicap.
Only then will connect the Lb's with signals.

Kind regards,

Benjamin Voelzke
4 REPLIES

Re: Seeking a solution for the automatic connection mapping function.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

could you please tell us which product you are using (Plant Simulation, Process Simulate, FactoryCAD, ...)?

 

Thanks,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Seeking a solution for the automatic connection mapping function.

Gears Phenom Gears Phenom
Gears Phenom

I search a solution for Process Simulate.

 

thanks

Kind regards,

Benjamin Voelzke

Re: Seeking a solution for the automatic connection mapping function.

Gears Phenom Gears Phenom
Gears Phenom

I have heard that there are at Siemens considerations as a tool to develop.
If so, there may be a beta version?
I urgently need the tool for the virtual commissioning.

Kind regards,

Benjamin Voelzke

Re: Seeking a solution for the automatic connection mapping function.

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

 

does anyone have a solution for this?