11-10-2017 11:36 AM
I'm running Process Simulate 13.0 with FANUC RCS. Given an existing robot path, I would like to specify a different tool frame for a via while preserving the current robot position. Currently, when I change one of the various "Utool" columns in the "Path and Locations" editor, the robot physially adjusts itself to make the existing via match the new TCP.
What is the best way to make this frame shift? My current, inefficient workaround is to change all the via's "Def Type" to "Pose" and download the listing file. Then I change the tool frame number in the listing file and upload it back into ProcessSimulate. Finally, change the Def Type back to Cartesian.
There must be a better way!
Solved! Go to Solution.
11-10-2017 11:51 AM
**bleep** Locations By Tcp Offset from Olp Tool package is meant for that.
<<
>>
11-10-2017 03:29 PM
Great. This is exactly what I needed. I was unaware of the OLP Tool package. I have found the installer on the GTAC FTP server.
Thank you!
Watch Replays of Previous Topics