Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulation with gripper is not performed after closing and re-opening the saved cell.

Experimenter
Experimenter

Hello,

 

I am using RobotExpert 13.0 trial version and fidning some difficulties regarding the Gripper.

 

The problem is the gripper is not recognized, after saving and reopening the same cell. The gripper is defined in Tool Defination also. 

 

The simulation will work fine with robot movement as well, but the gripper will be constant. 

 

Can you please help me solving the problem? 

 

Thank & Regards,

Gowtham H N 

wipro Ltd 

1 REPLY

Re: Simulation with gripper is not performed after closing and re-opening the saved cell.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

Take a backup of the griper file, delete file from the library Insert newly converted gripper file into RobertExpert and define it properly as gripper. 

Best Regards,
Jeethan Rohan