Cancel
Showing results for 
Search instead for 
Did you mean: 

Swept Volume Performance in Tecnomatix 14.0

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello.


In New Features Presentation for Tecnomatix 14.0 I have seen information that in new version Swept Volume tool should use Multi-threaded algorythm. But when I run swept volume for many operations in Tecnomatix 14.0 it still use only 1 case of CPU. So for that I want to ask if I need to turn Multi-threading on ?

4 REPLIES

Re: Swept Volume Performance in Tecnomatix 14.0

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello,

 

Unfortunately, it is a mistake in the presentation. The improvements that were made are not related to multi-threading. This is something that we will look into in future release.

 

Regards,

Yuval

Re: Swept Volume Performance in Tecnomatix 14.0

Experimenter
Experimenter

OneCore.jpg

Nice creativity by "Tobias"

Re: Swept Volume Performance in Tecnomatix 14.0

Creator
Creator

1whesr.jpg

Re: Swept Volume Performance in Tecnomatix 14.0

Experimenter
Experimenter

17% CPU utilization using a 6-core Xeon workstation running swept volumes.  LOL