cancel
Showing results for 
Search instead for 
Did you mean: 

Swept volume from device operation?

Valued Contributor
Valued Contributor

Hi everyone,

 

Im using TX 10.1 PS+PD.

 

is it possible to ge the volume from a device operation? For example a rotating fixture with a part on it?

 

Greetings,

Julian

2 REPLIES

Re: Swept volume from device operation?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

as far as I know, Swept Volume works only with robots and the stuff that is mounted to them.

 

Dave

Re: Swept volume from device operation?

Siemens Legend Siemens Legend
Siemens Legend

as workaround, you should be able to define the turn table as robot. Swept volume would then work. This is probably worth an ER.

 

best regards

Bernard