Cancel
Showing results for 
Search instead for 
Did you mean: 

Tecnomatix 13.0 Robot signal Aliases

Valued Contributor
Valued Contributor

Hi

 

I believe there is a new feature in version 13.0 which now allows the possiblility to have both $INHOME1 and the actual signal number $OUT[8]. What is the procedure to have this functionality?

 

Thanks

 

 

4 REPLIES 4

Re: Tecnomatix 13.0 Robot signal Aliases

Siemens Phenom Siemens Phenom
Siemens Phenom

You just need to have the .src or .dat file with the signal mapping definition loaded via Robot Setup / Explicit Data Upload, and define either signal (but not both) in Process Simulate.

Re: Tecnomatix 13.0 Robot signal Aliases

Valued Contributor
Valued Contributor

Hi

Thanks, I have tested and it seems to work well. Does the line SIGNAL UserNumSig $IN[65] TO $IN[72] also work? If so how does this relate to the signal viewer?

 

Regards

 

Re: Tecnomatix 13.0 Robot signal Aliases

Valued Contributor
Valued Contributor

Hi

 

Would it be like this?

Capture.PNG 

Re: Tecnomatix 13.0 Robot signal Aliases

Siemens Phenom Siemens Phenom
Siemens Phenom

Only boolean signals alias has been implemented, not the mapping of several boolean signals to integer signal.