Cancel
Showing results for 
Search instead for 
Did you mean: 

[Tecnomatix.Net]Customization to filter the Geometric Gun Search result?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello Everyone,

 

Customer is asking if he can write a customized program to do what Geometric Gun Search did plus additional filtering rules. Basically the idea is:

1. Perform Geometric Gun Search

2. Based on the Gun Search result, perform additional checks (e.g. the distance between floor and the gun handle) against those guns which pass the collision check.

 

Is this possible with Tecnomatix.Net?

 

Thanks

2 REPLIES

Re: [Tecnomatix.Net]Customization to filter the Geometric Gun Search result?

Legend
Legend

Hi,

 

you could create you own geometric gun search function that includes additional search filters or rules.

With the aid auf TX.Net API it is possible to do this.

 

But it is not possible to use the existing geometric gun search function.

 

Re: [Tecnomatix.Net]Customization to filter the Geometric Gun Search result?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Thanks for the info.