Cancel
Showing results for 
Search instead for 
Did you mean: 

Tecnomticx process simlation Event base simulation

Creator
Creator

Im doing a university project using tecnomatix PLM. It is arc welding robot cell. First I create cell in standard mode and simulate it base on time sequence . Next step is do event base simulation. I don’t have knowledge on part appearance, material flow handballing. Anyway my problems have describe bellow.

My problem is I can’t open the process simulate file with operations hierarchy in line simulate mode. (for develop CEE )

Error message1.jpg

As screen shot shows its gives study contains one or more operations which are not descendants of station. ( https://www.youtube.com/watch?v=83QDzAIwMII&feature=youtu.be ) captured video.

Error message1

  • Correct the operation hierarchy and try again.// I don’t know how to correct hierarchy.

So I delete all the operation and try to open files in line simulation mode. I could open the file in line simulation mode. When I again develop the process (jig operation and weld operation [ but weld part s disappear so I could not give weld location for weld operation]) It not allow to save the file and following error message gave.

 

Error message2 ( http://youtu.be/83QDzAIwMII ) // pls watch a 1min for error.

error 2.jpg

As screen shot shows its gives study contains one or more operations which are not descendants of station.

After that I create material floor operation. But I don’t know how I can update resources part as screen shot show.

(https://www.youtube.com/watch?v=T933w5AxC44&feature=youtu.be) pls watch 3.09min for error

 

questions

  1. My first question is how can I correct the operation hierarchy as error message show to me in standard mode. If so I should be able to open the file in line simulation mode with jig operation and robot weld operations.
  2. How can I update material flow and part appearance for weld operation?. (When weld operation begin part should be appear. But I don’t know how to handle part appearance. )
  3. How can I change the layout to advance simulation layout in line simulation mode.?

 

 

2 REPLIES

Re: Tecnomticx process simlation Event base simulation

Gears Phenom Gears Phenom
Gears Phenom

hello,

 

i think the problem is the operation structe.

you can only change to line simulation mode with Twin Object PR_OPStation.

 

Without Twin Object you have a problem

 

 

Kind regards,

Benjamin Voelzke

Re: Tecnomticx process simlation Event base simulation

Genius
Genius

Hello,

The problem is that the Station node is missing - but it doesn't have to be a twin object.

I only use "PR_StationProcess" objects and it works fine, but i'm not sure whether that obejct is present OOTB or only in our customization.

 

/Andreas