Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool Definition objects

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I'm trying to define a tool that I can use to trace a CLSF file.  It's not clear what objects need to be in place to do this.

 

Is a tool a part or a resource?

Do I need to assign kinematics to it?

Will it contain a frame?

 

When I select my part, the tool definition button is not active.  So I'm obviously not clear on the requirements for a tool.

1 REPLY

Re: Tool Definition objects

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Typically a resource is defined as a tool.  Open your resource for modeling, Go to Kinematics - Tool Definition.  The application will assign dummy kinematics if required.  It is good practice to model a frame at the tcp.  Save your modeling, use Mount command to attach to the robot and set the tcp.