Cancel
Showing results for 
Search instead for 
Did you mean: 

Transition in Line Simulation mode

Valued Contributor
Valued Contributor

Hi everyone,

 

I have a short question for Transition in Line Simulation mode. When I use "operation_end" for transition, the signal is only pulsed. What do I have to to use when I want to use two different operation ends which does not exactly end at the same time?

 

Is the RE-Option stored?

1 REPLY

Re: Transition in Line Simulation mode

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

hello,

 

the operation end signal is a pulse signal.

you can store the signal with logic blocks (SR or RS function)

 

other solution:

you can connect the operation ends of all operation to same time (connect all op with next op)