Cancel
Showing results for 
Search instead for 
Did you mean: 

Tx10.1; SignalMappingTool - error

Genius
Genius

Hello,

 

Im trying to import an excelfile with signals mapped to a smart component. When importing the signals i get the following error message in the log file:

===============================ERRORS===============================

Old format or invalid type library. (Exception from HRESULT: 0x80028018 (TYPE_E_INVDATAREAD))

 

The file I am trying to import is an .xlsx file, and it is attached. Can not really see what is wrong with the file...I had to attach it in a zip-file because the community complained that the xlsx was not really an excel file so the format of the file must include some errors.

 

BR

Andreas

 

2 REPLIES

Re: Tx10.1; SignalMappingTool - error

Gears Phenom Gears Phenom
Gears Phenom

hello.

in the picture you can see a working file.

works in PS10.1 and 11.1

 

please try with excel sheet in "xls" format (Office 2003)

 

Connection_mapping

Kind regards,

Benjamin Voelzke

Re: Tx10.1; SignalMappingTool - error

Genius
Genius

I noticed that in Tx11.1 the file works fine - but since that installation is on another client i am suspecting that the error is with my excel and not Tx10.1.
We can consider this closed... Smiley Happy