Cancel
Showing results for 
Search instead for 
Did you mean: 

Upload Default robotic program for Robcad

Valued Contributor
Valued Contributor

Hello guys!

 

I have the PROCESS version 11.1TR3
I downloaded the program in default module.

But I could not load the program in Robcad version 9.1, because the process Template Program is this "default.tpl" :

 

// File : <FileName>
//
// Generated with : <TecnomatixSoftware>
//
// Study : <Study>
// Robot : <RobotName>
//
// Author : <UserName>
// Date : <Date> - <Time>
//
DATA

<Data>

END_DATA

PROG <ProgName>

<Body>

END_PROG

 

Is there a default template, so when I download the program in the process, can I load it in Robcad?

Or is there any procedure that I can carry out of the process for Robcad?

3 REPLIES

Re: Upload Default robotic program for Robcad

Siemens Phenom Siemens Phenom
Siemens Phenom

You need to use an actual controller (Abb, Kuka, Fanuc, etc...) to transfer programs from Process Simulate to Robcad. For instance downloading with Abb-Rapid on Process Simulate and uploading with s4_spot on Robcad.

 

 

Re: Upload Default robotic program for Robcad

Pioneer
Pioneer
Hello,
you know that we can upload the default program from robcad to PS in that we use the default template of robcad, so you can try to use the default controller template of robcad to replace of PS and then download program for robcad.
it is just a suggestion without witness, you can try, but the first choice and correct way is described by expet GillesVelay.

best wishes
paul

Re: Upload Default robotic program for Robcad

Valued Contributor
Valued Contributor

Ok.

 

 

First I'll edit the default file I downloaded from PS, to the default of the Robcad and try to upload in Robcad.

 

And then I will do with the robot module.

 

Thanks!