Cancel
Showing results for 
Search instead for 
Did you mean: 

[VS2013] Add/delete Tecnomatix controls

Legend
Legend

Hi,

 

I want to get familiar with the Tecnomatix.Engineering.UI controls. Therfore I use C#, Visual Studio 2013 and Version 11.1 of the Tecnomatix applications (Process Simulate)

I added the controls to Visual studio as it is decribed in the SDK help.

But when I drag and drop a control to the form, I mostly get an error that Tecnomatix.Engineering dll is not found. (see Add.png)

I also get an error if I want to delete a control on the form (see Delete.png)

 

What am I doing wrong?

What other dlls should be added as a reference in a project?

 

2 REPLIES

Re: [VS2013] Add/delete Tecnomatix controls

Legend
Legend

Hi Markus,

 

I´m not 100% sure, but TX controls with V11.1 only work in 32bit version of PS.

 

With 11.1 TR3 or higher you can use the TX controls of the 64bit version.

 

I started with 11.1TR3 without any problem. The same with all versions after that (12.x)

 

Regards

Re: [VS2013] Add/delete Tecnomatix controls

Legend
Legend

Hi Patrick, thank you for the reply.

 

That is what I suspected after I read this thread.