Cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual Commissioning PS to access OPC server

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello guys,

 

I have been trying to connect to a PLC from PS 10.1 via an OPC connection.

The laptop PS is installed on, is connected with ethernet cable to a switch, and the network adapter of the PLC is also connected to the switch.

 

The problem is that PS client can't see the OPC server.

I have tried to install the OPC server on another machine, and connect it to the switch but, the result is the same, PS can't see the OPC server.

How can this connection be made?

 

 

10 REPLIES 10

Re: Virtual Commissioning PS to access OPC server

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hallo,

 

Ich habe die Installation auf meinem 10,1 PS Maschine der OPC-Server ( http://industrial.softing.com/).

Unterhalb der OPC- Einstellungen , kann ich den OPC-Server auszuwählen.

 

Der OPC-Server muss mit der SPS konfiguriert.

 

Inator

 

PS PLC Optionen

 

 

 

  

 

Kind regards,

Benjamin Voelzke

Re: Virtual Commissioning PS to access OPC server

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hallo,

 

Danke für Ihre Vorschlag, ich habe die softing OPC Server installiert und ausprobiert.
Der OPC Server kommuniziert mit der SPS; in die Verbindungsliste, hab ich der korrekte OPC Server Link(136.129.1.11 - PLC; 136.129.1.12 - lokal), aber in PS OPC Browser noch keine Verbindung unter Local Server(s).

OPC_server.jpg

 

Kind regards,

Endre

 

Re: Virtual Commissioning PS to access OPC server

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

hello,

 

my operation system: windows 7 prof. x64

process simulate 10.1 (64bit)

 

on my system i see the local opc server.

 

sorry

Re: Virtual Commissioning PS to access OPC server

Legend
Legend

hi,

 

i think during the installation of INAT OPC server, something went wrong.

During the installation process some additional installations are performed in background.

Please make sure, every thing is installed correctly.

 

You can try to use the "OPC Test Client" of the INAT software to check if there is an OPC server available.

 

 

Re: Virtual Commissioning PS to access OPC server

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello guys,

 

Thank you for the help and assistance, it turns out that I had a license problem.

 

Best regards.

Highlighted

Re: Virtual Commissioning PS to access OPC server

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

I have the license now for VC, but still no connection appears in PS.

The softwares I have been trying with are RSLinx and INAT OPC Server.

I noticed that all these OPC Server softwares are installed under C:\Program Files (x86).

Meaning that they are 32bit applications. My Process Simulate is a 64bit application.

Does this affect the fact that the OPC connection is not visible in PS?

When I test the connection in the test Client it shows that the connection is good, but in PS I can't validate any connection.

Should I install a 32bit PS?

 

Thanks,

Endre

Re: Virtual Commissioning PS to access OPC server

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

hello,

 

i have installed PS as 64bit software

inat opc is installed as 32 bit software.

 

on my machine i can select the opc server in process simulate.

 

i haven't done any other settings for OPC.

Kind regards,

Benjamin Voelzke

Re: Virtual Commissioning PS to access OPC server

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

Thank you guys for the tips, i managed to connect to the PLC via OPC.

The problem was that i didn't have installed the OPC Core Components Redistributable (x64).

OPC_running.jpg

 

Best regards,

Re: Virtual Commissioning PS to access OPC server

Pioneer
Pioneer

Hi,

 

I'm having a similar problem, but I have the OPC Core Components installed.. But still can't see any of the OPC servers running..

 

I have tried 3 different OPC servers. All with the same result.

I used:

- Kepserver OPC

- INAT OPC

- Matrikon OPC

 

I'm hoping to try Simatic OPC today but I don't think it's the OPC server..

 

Any ideas anyone?

Best regards,

Gabriel