Cancel
Showing results for 
Search instead for 
Did you mean: 

can't save the PS simulation elements back to TC

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

if i open the ps from the TC, i can load every object like resources, part ,that's look good!

1.png

but if i created some object in PS, do some simulation , and update to TC, then error happend

2.png

find some erro message as below:

2016-06-28_18-29-16.png

 what i need to do?

 

Teamcenter9.1

Tecnomatix_10.1

Tecnomatix_10.1_TC_Alignment-16-x64

1 REPLY 1

Re: can't save the PS simulation elements back to TC

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi!

 

Personally I think it's better to author structures in Teamcenter, not in Process Simulate.

Which objects did you create? A message like this sometimes happens when Teamcenter cannot understand the data provided by Process Simulate correctly.

 

TC Error 203341 means: Missing BOM Line.

I think if you've created a robot, Teamcenter does not understand in which structure to place it.

 

You can try to create Workarea to use it for Resource structure in Teamcenter. Assign this workarea to the process. Create new Resources under workarea, not as a root node in Process Simulate. Maybe it works.

Regards, Vladimir.