Cancel
Showing results for 
Search instead for 
Did you mean: 

commissioning cell with process simulate 11.1

Gears Phenom Gears Phenom
Gears Phenom

today i load a virtual commissioning cell in process simulate 11.1

process simulate is connected via simba box to the plc SIEMENS 416F.

 

problem:

under ps10.1 runs the cell without problems (connect plc over OPC, or CEE)

under ps11.1 the robot have big problems with the standard program number

 

steps:

- the plc (over simba connections) send the program number to ps 11.1

- ps11.1 have problems to understand this number

- i force the number again to zero

- after the force ps mirror the prog number back to plc

- the plc jump to the next step

- plc send the start_program signal

- process simulate receives the signal in simulation panel

- the robot does not start (problem again)

- i force the signal again to zero

- after force the robot started

 

- robot drive to pick position and send signal to plc

- plc receive the signal and send release signal to robot (olp command "wait signal")

- problem again

- robot wait and wait and wait

- in simulation panel is the signal from plc TRUE

 

unfortunately i don't have a commissioning lizenz for ps10.1

 

 

 

Kind regards,

Benjamin Voelzke
2 REPLIES

Re: commissioning cell with process simulate 11.1

Gears Phenom Gears Phenom
Gears Phenom

i have check the cycle time from my plc

 

2 ms

 

i think this is to fast for PS with profinet simba connection

 

i have created a IR1968327

Kind regards,

Benjamin Voelzke

Re: commissioning cell with process simulate 11.1

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Hotfix 14 fix the problem.

 

thanks