Cancel
Showing results for 
Search instead for 
Did you mean: 

download / upload with default controller

Valued Contributor
Valued Contributor

Hi,

 

i need to download my programm with the default controller with Process Simulate.

And then upload this programm in Robot Expert.

 

It ist possible , and when how ?

 

Thanks.

 

 

7 REPLIES 7

Re: download / upload with default controller

Siemens Phenom Siemens Phenom
Siemens Phenom

There is currently no upload in the default controller. A workaround would be to use a specific OLP controller (some do not require additional licenses).

Re: download / upload with default controller

Valued Contributor
Valued Contributor

hi,

 

this is the correct way.

i use now my krc controller for download and upload.

thanks.

Re: download / upload with default controller

Creator
Creator

Hi,

I tried Upload with the Krc but it complains about not having a licence. Could you tell me which controllers don't require a licence for Upload.

 

Re: download / upload with default controller

Siemens Phenom Siemens Phenom
Siemens Phenom

I'm afraid, besides the default controller there is no license-free controller.

Re: download / upload with default controller

Creator
Creator

Hi, apparently, all controllers require a licence so this is not an option. I will attempt to use the Default Robcad format uploader. Unfortunately all my robcad examples went with my old SGI machine! Could someone give me a robcad default download example please?

Thanks..

Re: download / upload with default controller

Siemens Legend Siemens Legend
Siemens Legend

FYI: Version 13.1 (release around December 16')  will include a new feature: Upload with Default Controller.

Then you can download from PS and upload into RBX as you wanted. 

 

Kind regards,
Gal Snir

Re: download / upload with default controller

Creator
Creator
Kool. Thanks!