Cancel
Showing results for 
Search instead for 
Did you mean: 

eM-Server Update error while updating with System Frames like Base Data and Tool Data

Pioneer
Pioneer

 

 

 

mac_data_err.PNGerror

Hello,

 

Im getting the above error while Im updating the server with Base data and Tool Data using Kuka Machine data files.

 

Following is the process I have followed.

 

- From Robot Properties> Selected KRC> KRC5.6 R02> 5.6 (versions for controller)

- Robot Setup> loaded the machine data

- applied the new base data and tool data from Tool & Base option

- Create/Update System Frames> updated to Mada file

- Initialized the RCS (Everything went fine)

- Updated the server, but Im getting the above error.

 

Please let me where Im going wrong and suggest the solution.

 

Thanks in Advance,

Ram

1 REPLY

Re: eM-Server Update error while updating with System Frames like Base Data and Tool Data

Siemens Phenom Siemens Phenom
Siemens Phenom

Your eMServer schema is missing the import of the robotics customization: InitData/RoboticsCust