Showing results for 
Search instead for 
Do you mean 
Reply

error in open ArcWeld_demo_abb when using robotexpert

Hi,

When I open the new cell from documentation in robotexpert, it can not show the whole model, it showed some components are not defined. But the cell is in the documentation which i got from siemens. Can someone help me to solve this problem?

Thank you for help.

 

2 REPLIES

Re: error in open ArcWeld_demo_abb when using robotexpert

[ Edited ]

I think that you don't have correctly defined Library folder. The example cell is provided with a short install manual in MS Word. You should check it.

 

Dave

Re: error in open ArcWeld_demo_abb when using robotexpert

Hi,

Thank you for your answer, I think it is the problem which due to the error.