Cancel
Showing results for 
Search instead for 
Did you mean: 

kinematic speed

Gears Phenom Gears Phenom
Gears Phenom

the speed in the kinematics editor is referring to mm.(milimeter) (configuarte under options)
Which relation is it to the millimetre? (what time?)

 

2014-04-13 10_52_35-Kinematics Editor -  sf_6028344_1750x2100_l.png

Kind regards,

Benjamin Voelzke
1 REPLY

Re: kinematic speed

Siemens Legend Siemens Legend
Siemens Legend

Hi Benjamin.

I had a look at the Documentation under "To create joints:" and found this:

"

9. In the Speed field, enter a value for the speed of the joint (Linear: mm/sec, Angular: rad/sec).

10. In the Acceleration field, enter a value for the acceleration of the joint (Linear: mm/sec^2,
Angular: rad/sec^2).

"

Kind regards,
Gal Snir