Cancel
Showing results for 
Search instead for 
Did you mean: 

line tracking with process simulate

Gears Phenom Gears Phenom
Gears Phenom

hello everybody,

 

i work in the last days with line tracking project.

 

i have a question about the ps functionality?

 

in my test's i see no chance to syncronise the conveyor speed with the robot tcp speed?

it is possible?

 

i can change the speed for conveyor but the robot move with tcp speed.

in all my cases i must test the syncronisation about the reachability and time / speed of conveyor per hand?

is this correct workflow?

 

in my eyes "the wait wobj function" for abb is only for wait for start the robot path.

 

thanks

Kind regards,

Benjamin Voelzke
9 REPLIES

Re: line tracking with process simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Do you work with ABB RCS Module ? Line Tracking is supported with RRS, but not yet in MOP / RCS Disconnected.

Re: line tracking with process simulate

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

yes i work with RCS Modul.

 

in my case the part fly with a material flow on conveyor.

on reachability position i start the robot path.

but it is very hard to find the correct time interval to start the robot between conveyor.

Robot Starts is easy.

but the robot move ex. with Speed V1000 the lines

with Speed V1000 i must find the correct conveyor speed (or Object flow speed) to sync these 2 operations.

 

line.jpg

Re: line tracking with process simulate

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

hello,

 

ABB with line Tracking:

 

Do i work with spezial ABB Machine Data for Line Tracking?

In my case i drive with standard ABB Machine Data. (no ext. axes)

 

 

 

 

 

 

 

Re: line tracking with process simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Off course, you need dedicated machine data with a conveyor mechanical unit defined inside.

Re: line tracking with process simulate

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

over which signal brigde send PS the position to RCS Machine Data?

where can i configurated these?

Re: line tracking with process simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

The concept of line tracking in Process Simulate is hopefully explained in the manual (see Robot Properties / Conveyor).

Re: line tracking with process simulate

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

I`m trying start a project with line tracking. I´m working with Yaskawa controller but without RCS connected. Is posible work with line tracking and without RCS in Process Simulate Standalone v13.1.2 or v14.0.2 ???

Please help!

Re: line tracking with process simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

There is currently no support for line tracking in MOP (without RCS).

Re: line tracking with process simulate

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

thanks very much for the quick reply.