Cancel
Showing results for 
Search instead for 
Did you mean: 

modeling with robot dosen't work

Gears Phenom Gears Phenom
Gears Phenom

I can open currently no robot to the modelling (see picture)

I've tried it with ABB and KUKA.

all components are *.cojt

 

i have tested with PS 10.1 and PS 11.1

 

test with connected study

test with disc. study

 

always with the same message

 

modeling_problem.jpg

 

Kind regards,

Benjamin Voelzke
1 REPLY

Re: modeling with robot dosen't work

Legend
Legend

Modelling for robots works correctly for robots without dresspack (fupa).

 

For newer robot models, which include a fupa, the modelling does not work.

 


I have tried modelling for an ABB and a KUKA robot without fupa. Both are working.

I also tried an ABB and KUKA with fupa and here it is not working.

 

Process Simulate.jpg

 

Have a try with my files (attachment).