Cancel
Showing results for 
Search instead for 
Did you mean: 

new function for olp command "comment out line"

Gears Phenom Gears Phenom
Gears Phenom

a request for olp command:

 

"comment out line"

 

example: KUKA robot olp command

firstdress()              -> call another path

 

after pressing the button

; firstdress()            -> command is change to comment

 

i have no problem to drive the path

 

(big problem for this situation is autoteach)

 

Kind regards,

Benjamin Voelzke
5 REPLIES

Re: new function for olp command "comment out line"

Siemens Phenom Siemens Phenom
Siemens Phenom

There is new HF217 on top of Tecnomatix 10.1 which introduces a "Ignore Logic" setting in Options / Motions.

When this option is turned on, all logics, including calls to paths or routines, are skipped. This new facility might answer your need.

Re: new function for olp command "comment out line"

Gears Phenom Gears Phenom
Gears Phenom

the HF217 is working

 

but my problem is,it is not possible to comment out custom xml olp commands

 

in this case i copy the logic to notepad and comment out the logic and copy back to ps

 

 

 

 

Kind regards,

Benjamin Voelzke

Re: new function for olp command "comment out line"

Siemens Phenom Siemens Phenom
Siemens Phenom

logic inside custom XML will also be ignored if this new motion option is turned on

Re: new function for olp command "comment out line"

Gears Phenom Gears Phenom
Gears Phenom

sorry

the ignored function is not the problem

 

the problem is:

i will run the simulation with signals and logic

but not all lines in olp command

 

logic without custom xml can change over free text editor

but logic with custom xml can not change (comment out) other free text editor

 

 

Kind regards,

Benjamin Voelzke

Re: new function for olp command "comment out line"

Gears Phenom Gears Phenom
Gears Phenom

i have created a ER.

 

ER 1955493

Kind regards,

Benjamin Voelzke