Cancel
Showing results for 
Search instead for 
Did you mean: 

part material flow

Valued Contributor
Valued Contributor

Hello, 

I am using tecnomatix 13.1.1. and i have a problem within a Event Based simulation in line simulation mode. 
First, i am not sure if i can the define the problem exaclty. Basicly no part is shown when my simulation is started. 

 A part  or some of parts is can be seen only in "apperances" in object tree. but its icon has "cross". 

I think I realy need a basic knowledge of how to use "material flow viewer". 

I read everything about material flow in help menu but i could not succed it. I need your help. 

Thanks. 

1 REPLY

Re: part material flow

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Burpee,

actually there is no obvious mistake in your screenshot.

You have an INIT step and hopefully parts are assigned to the ops in your Mat-Flow-Viewer.

 

Also the fact, that you get appearances instead of parts is correct.

Parts do not exist in CEE, only appearances.

 

But appearances having a cross, ist really strange.

Are you sure the corresponding parts are correctly displayed also when loading as time-based study?