Showing results for 
Search instead for 
Do you mean 
Reply

problem with tools

I am using the program robotexpert, and I cannot load any tool, in an example program I see 2 folder (grippers and weldtorches) but tell me the file tipe is not supported.

As I can discharge myself tools.

4 REPLIES

Re: problem with tools

[ Edited ]

Hello,

 

what version of the RE do you use? (release no., trial vs. full)

 

In general, the components can be inserted through Modeling - Insert Component From File command. All components have to be under the library root and they are saved in file system as folders with .COJT extension.

 

Dave

Re: problem with tools

I am using a version 30 days. I have been able to pass it through cad converter, and he already appears me in the work panel. Can I get librarys of tools, to practice with them?

Re: problem with tools

[ Edited ]

Ok. I think that the best way for you should be to browse the Add-Ons folder in the install data of the RE. Among other things, the Add-Ons folder contains the Libraries (just copy it to your Library root), the ExampleCell (good start for beginners with short install manual). Furthermore, browse the Documentation folder in the install data. I suggest RobotExpertQuickStartGuide.pdf and QuickStart_Movies.

 

(I'm not familiar with the trial version, but I'm convinced that it will be the same as in the full ver.)

 

Good luck with RobotExpert testing Smiley Happy

 

Dave

Re: problem with tools

ok, Thanks you